Academic Program

Setup

Setup

Step by Step Instructions

Using MPLAB® Code Configurator (MCC), this project generates the code to blink an LED using a hardware Timer0 interrupt to generate the delay between the on and off state.

proj6bd.jpg

 

The project uses:

  • PIC16F18875
  • HPC Curiosity Board
  • MPLAB X IDE
  • MPLAB Code Configurator (MCC) plug-in
  • MPLAB XC8 Compiler

​

To follow along with these steps, MPLAB X should be open and the HPC Curiosity Board connected to the computer through a USB cable.

Step 1 - Create a new standalone project in MPLAB X for a PIC16F18875.

​

If this is your first time creating an MPLAB X project, please visit the "Create a Standalone Project" page to follow step-by-step instructions on how to do this.

Step 2 - Open the MPLAB Code Configurator under the Tools > Embedded menu of MPLAB X IDE.

mcclaunch.png

 

Step 3 - Select the peripherals for your project. For this project, the following peripherals need to be selected:

  • System Module
  • Interrupt Module
  • Pin Module
  • TMR0

These modules will automatically be included when you launch the MCC, with the exception of TMR0. TMR0 needs to be added from Device Resources. Just click on Timer and then double click on Timer0 to add it to the project. The result should look like the picture below:

projectmenu.png