Academic Program

Program the PIC16F18875 Device

Program the PIC16F18875 Device

Step 11 - Make sure your project has the Curiosity Board selected and a USB cable is connected to the board.

Click on Make and Program Device. This will build the project again and launch the programmer. In the Output window, you should see a series of messages and, if successful, it will end with a "Programming/Verify complete" message.

Main_Program_Target_Project.png

 

Output Window:

Connecting to MPLAB PICkit 3...
Firmware Suite Version.....01.34.11
Firmware type..............Enhanced Midrange

Target detected
Device ID Revision = 6

The following memory area(s) will be programmed:
program memory: start address = 0x0, end address = 0x7ff
configuration memory
Device Erased...

Programming...
Programming/Verify complete

The D2 LED connected to RA4 will be blinking on the HPC Curiosity Board.
 
proj1final.png
​

If it's the first time the programmer is connected to the board, the programming tool may need to download the proper operating firmware for the exact device. You may see a series of processes if this occurs. This should only happen once:

Downloading Firmware…
Downloading bootloader
Bootloader download complete
Programming download…
Downloading RS…
RS download complete
Programming download…
Downloading AP…
AP download complete
Programming download…
Firmware Suite Version…..01.34.11
Firmware type…………..Enhanced Midrange

Step 12 - The project can be closed in MPLAB X IDE. The project is saved automatically when it is built, but any changes to files or configuration may ask to be saved before the project is closed.

The project can be closed under the File Menu > Close Project.

closeproject.png