Academic Program

Setup

Setup

Step by Step Instructions

Using the MPLAB® Code Configurator (MCC) simplifies the setup for the various registers within the device to create a digital input. To demonstrate how to get started, this project monitors a momentary switch connected to pin RB4 that is enabled as a digital input using an internal pull-up. The code will light an LED connected to RA4, enabled as a digital output when the switch is pressed.

proj2pic.png

 

The project uses:

  • PIC16F18875
  • HPC Curiosity Board
  • MPLAB X IDE
  • MPLAB Code Configurator (MCC) plug-in
  • MPLAB XC8 Compiler
​

To follow along with these steps, MPLAB X IDE should be open and the HPC Curiosity Board connected to the computer through a USB cable.

Step 1 - Create a new standalone project in MPLAB X for a PIC16F18875.

​

If this is your first time creating an MPLAB X project, please visit the "Create a Standalone Project" page to follow a step-by-step instruction on how to do this.

Step 2 - Open MCC under the Tools > Embedded menu of MPLAB X IDE.

mcclaunch.png

 

Step 3 - Select the peripherals for your project. For this project, the following peripherals need to be selected:

  • System Module
  • Interrupt Module
  • Pin Module

The System Module, Interrupt Module, and the Pin Module will all be automatically included when you launch the MCC. The result should look like the picture below:

proj1per.png