Program
Step 12 - Make sure your project has the Curiosity Board selected and USB cable is connected to the board.
Click on Make and Program Device. This will build the project again and launch the programmer. In the Output window, you should see a series of messages and, if successful, it will end with a "Programming/Verify complete" message and the D2 LED connected to RA4 will be lit when the potentiometer is turned to the right of center on the HPC Curiosity Board.
Output Window:
Connecting to Starter Kit on Board...
Currently loaded firmware on Starter Kit on Board
Firmware Suite Version.....01.54.00
Firmware type..............Enhanced Midrange
Target voltage detected
Target device PIC16F18875 found.
Device Revision ID = 2002
Device Erased...
Programming...
The following memory area(s) will be programmed:
program memory: start address = 0x0, end address = 0x7ff
configuration memory
Programming/Verify complete
The D2 (RA4) LED will light up when the potentiometer is turned clockwise more than the half-way point. The picture below shows the potentiometer beyond the half-way point so the LED is lit.

If it's the first time the programmer is connected to the board, the programming tool may need to download the proper operating firmware for the exact device. You may see a series of processes if this occurs. This should only happen once.
Downloading Firmware…
Downloading bootloader
Bootloader download complete
Programming download…
Downloading RS…
RS download complete
Programming download…
Downloading AP…
AP download complete
Programming download…
Firmware Suite Version…..01.34.11
Firmware type…………..Enhanced Midrange
Step 13 - The project can be closed in MPLAB X IDE. The project is saved automatically when it is built, but any changes to files or configuration may ask to be saved before the project is closed.
The project can be closed under the File Menu > Close Project.