Academic Program

System Module

System Module

Step 6 - Next, the system needs to be set up. Click on System Module in the Project Resources list. It should be highlighted in blue when selected.

system.png

 

In this section, the oscillator settings and the configuration settings are selected.

Oscillator

  1. Select the HFINTOSC from the Oscillator Select drop-down menu.
  2. Select the 4MHz selection from the HF Internal Clock drop-down menu.
  3. Select Clock Divider value of 4.

This will enable the internal 1 MHz internal oscillator as the system clock.

oscillator.png

 

Also, make sure the Low-voltage Programming Enable mode is selected at the bottom of the System Module screen.

lvp.png