Academic Program

Create an MPLAB X Project

​Create an MPLAB X Project

 

Note: To follow along with these steps, MPLAB X IDE should be open and the HPC Curiosity Board connected to the computer through a USB cable.

Step 1 - Create a new standalone project in MPLAB X for a PIC16F18875.

​

Note: If this is your first time creating an MPLAB X project, please visit the "Create a Standalone Project" page to follow a step-by-step instruction on how to do this.

Step 2 - Open the MPLAB Code Configurator under the Tools > Embedded menu of MPLAB X IDE.

mcclaunch.png

 

Step 3 - Select the peripherals for your project. For this project, the following peripherals need to be selected:

  • System Module
  • Interrupt Module
  • Pin Module

The System Module, Interrupt Module, and the Pin Module will all be automatically included when you launch the MCC. The result should look like the picture below:

proj1per.png