System Setup
Step 6 - Close the Pin Manager. Next, click on System Module in Project Resources to open the center section.
In this section, the oscillator settings and the configuration settings are selected.
Oscillator
- Select the HFINTOSC from the Oscillator Select drop-down menu.
- Select the 4_MHz selection from the HF Internal Clock drop-down menu.
- Select a Clock Divider value of 4.
This will enable the internal 1 MHz internal oscillator as the system clock.
Also, check that the Low-voltage Programming Enable mode is selected at the bottom of the System Module screen.