Academic Program

System Module

System Module

Step 6 - The System Module needs to be set up next. Click on System Module under Project Resources.

system.png

 

In this section, the oscillator settings and the configuration settings are selected.

Oscillator

  1. Select the HFINTOSC from the Oscillator Select drop-down menu.
  2. Select the 4_MHz selection from the HF Internal Clock drop-down menu.
  3. Select Clock Divider value of 4.

This will enable the internal 1 MHz internal oscillator as the system clock.

oscillator.png

 

Also, make sure the Low-voltage Programming Enable is selected at the bottom of the System Module screen.

lvp.png