Interrupt & Exception Usage
PIC32MZ Interrupt and Exception operation must be carefully initialized by the application developer. This page summarizes the key initialization & usage steps required for both interrupt exceptions and general exceptions.
Further information regarding interrupt and exception usage is provided by the "MPLAB® XC32 User's Guide" (DS50001686)
Table of Contents
Step 1. #include Standard Headers
Step 2. Provide Interrupt Service Routine (ISR)
Step 4. Configure Interrupt Controller
Step 5. Assign Shadow Register Sets to IPLs
Step 6. Set Interrupt Controller Mode
Step 7. Enable Interrupt Exceptions
Code Example - Interrupt Usage
Code Example - General Exception Usage
Interrupt Exception Usage
PIC32MZ CP0 and Interrupt Controller registers are initialized by hardware and MPLAB® XC32 Compiler start-up code placing the CPU in the following state upon entry to your main() function:
- Ebase = _ebase_address (= 0x9D000000 for PIC32MZ2048ECG100)
- OFFx registers are initialized by start-up code based on defined ISRs in your project
- StatusBEV = 0 (Exception vector entry points changed from the "bootstrap" location to the "normal" location)
- General Exceptions: Ebase (=0x9D000000) + 0x180
- Interrupt Exceptions: Ebase + OFFx
- StatusIE = 0 (Interrupt Exceptions Disabled)
- StatusIPL<2:0> = 0 (CPU running @ priority level 0)
- INTCONMVEC = 0 (Interrupt controller configured for single-vector mode)
- Cache is enabled and configured in write-back with write allocation mode
The following steps must be taken in the application code for proper interrupt exception initialization & usage.
Step 1. #include Standard Headers
The application must include header files xc.h and attribs.h as shown below:
#include <xc.h>#include <sys/attribs.h>
The <sys/attribs.h> header file provides macros intended to simplify the application of attributes to interrupt functions:
- _ISR(V, IPL)
- _ISR_AT_VECTOR(V, IPL)
There are also vector number macros defined in the processor header files (included via <xc.h>) - see the appropriate header file in the compiler’s /pic32mx/include/proc directory.
Step 2. Provide Interrupt Service Routine (ISR)
An interrupt handler function is different from an ordinary function in that it handles the context save and restore to ensure that upon return from interrupt, the program context is maintained. A different code sequence is used to return from these functions as well.
There are several actions that the compiler needs to take to generate an interrupt service routine:
- The compiler has to be told to use an alternate form of return code.
- The compiler has to be told whether to use a shadow register set for context save/restore.
- The function needs to be linked to the interrupt vector.
Several function _attributes_ are provided to allow the application developer to define ISR handlers so that the compiler generates the correct code for an ISR (__ISR() macros are provided so that this is easier to accomplish).
For all interrupt vectors without specific handlers, a default interrupt handler will be installed. The default interrupt handler will reset the device.
An application may override the default handler and provide an application-specific default interrupt handler by declaring an interrupt function with the name _DefaultInterrupt.
Interrupt Service Routine Definition using the _ISR() Macro
void__ISR_AT_VECTOR(_INT_VECTOR_NUMBER, IPLx[SRSy|SOFT|AUTO]) isrName(void){/* Clear the cause of the interrupt (if required) *//* Clear the interrupt flag *//* ISR-specific processing */}
__ISR_AT_VECTOR:
Macro for defining an interrupt service routine such that the entire handler is placed at the vector address.
This macro is especially useful in PIC32MZ devices which feature variable vector offsets. The compiler calculates the required vector spacing and initializes OFFx registers accordingly.
_INT_VECTOR_NUMBER:
Unique Vector Number Macro from the device header file. Also listed in table 7-2 of the device data sheet as "XC32 Vector Name":
IPLx[SRSy|SOFT|AUTO]:
- Assign Interrupt priority level (0-7) to the ISR, and
- Define how context is preserved
- The generated code preserves context by either using a shadow register set (SRSy) or using generated software instructions (SOFT) to push context onto the stack.
The IPLx setting must match the interrupt controller setting (IPCx) for the specific interrupt source.
isrName:
Unique name you give the ISR.
NO parameters are allowed on an ISR. NO return values are allowed either.
void __ISR_AT_VECTOR(_INT_VECTOR_NUMBER, IPLx[SRSy|SOFT|AUTO]) isrName(void)
Example
In this example, we define a Timer 2 ISR function T2Interrupt() that is configured as an IPL-level-4 process, and which will use shadow-register set #3 (as defined by the PRISS register setting):
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationPRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
while(1);/* main application loop */
}
Step 3. Configure Peripheral
Next, you must configure the peripheral to generate interrupt request events.
For example, PIC32MZ contains several Timer peripherals modules. Each module has a period register (PRx) that when properly initialized, will periodically trigger a Timer interrupt request signal in an IFSx register as shown:
In this example, we will initialize Timer2 to generate interrupt requests every 100mS, given PB3CLK of 8 MHz (code not shown):
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
while(1);/* main application loop */}
Step 4. Configure Interrupt Controller
The next step is to configure the associated Interrupt Controller Flag, Enable and Priority settings for the specific interrupt. In this case, those registers/bits associated with Timer 2 interrupt events:
- IPC2 Register
- Contains Timer 2 interrupt priority bits
- IFS0 Register
- Contains Timer 2 interrupt request bit
- IEC0 Register
- Contains the Timer 2 interrupt enable bit
Refer to the Interrupt Controller section in the device data sheet for a complete description of IPCx/IFSx/IECx registers for all interrupt sources.
In the following example, we will configure these registers, setting the initial priority level of the Timer 2 interrupt event to 4, matching the IPL setting shown in the ISR function definition below.
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
IPC2bits.T2IP = 4;/* Set Timer 2 interrupt priority to 4 */IFS0bits.T2IF = 0;/* Reset the Timer 2 interrupt flag */IEC0bits.T2IE = 1;/* Enable interrupts from Timer 2 */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
while(1);/* main application loop */
}
Step 5. Assign Shadow Register Sets to IPLs
The PIC32MZ has seven shadow register sets that can be used for any priority level, eliminating software context switch and reducing interrupt latency.
If you assign a shadow register set to an interrupt handler function (as in our example), you must also initialize the PRISS (PRIORITY SHADOW SELECT) register.
The following example initializes PRISS so that shadow register sets 1-7 are assigned to interrupt priority levels 1-7 respectively.
Setting PRISS = 0x76543210; guarantees that each user interrupt priority level will have its own dedicated shadow register set.
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
IPC2bits.T2IP = 4;/* Set Timer 2 interrupt priority to 4 */IFS0bits.T2IF = 0;/* Reset the Timer 2 interrupt flag */IEC0bits.T2IE = 1;/* Enable interrupts from Timer 2 */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
while(1);/* main application loop */
}
Assigning a shadow register in an ISR definition without properly configuring PRISS will produce unpredictable behavior.
The "Shadow Registers" page provides more details on the shadow register set operation on PIC32MZ.
Step 6. Set Interrupt Controller Mode
Next, we need to configure the interrupt controller to operate in MULTI-VECTOR MODE, whereby each interrupt source is assigned to its own interrupt vector.
This setting is controlled by the INTCONMVEC bit.
MPLAB XC32 provides a nice macro that can be applied with the INTCONSET register as shown in the following example:
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
IPC2bits.T2IP = 4;/* Set Timer 2 interrupt priority to 4 */IFS0bits.T2IF = 0;/* Reset the Timer 2 interrupt flag */IEC0bits.T2IE = 1;/* Enable interrupts from Timer 2 */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
INTCONSET = _INTCON_MVEC_MASK;/* Configure Interrupt Controller for multi-vector mode */
while(1);/* main application loop */
}
Step 7. Enable Interrupt Exceptions
Next, we need to globally enable interrupts by setting the CP0 StatusIE bit.
MPLAB® XC32 provides a handy __builtin() function for this task:
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
IPC2bits.T2IP = 4;/* Set Timer 2 interrupt priority to 4 */IFS0bits.T2IF = 0;/* Reset the Timer 2 interrupt flag */IEC0bits.T2IE = 1;/* Enable interrupts from Timer 2 */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
INTCONSET = _INTCON_MVEC_MASK;/* Configure Interrupt Controller for multi-vector mode */
__builtin_enable_interrupts();/* Set the CP0 Status register IE bit high to globally enable interrupts */
while(1);/* main application loop */
}
Step 8. Enable Peripheral
Finally, we trigger the generation of interrupt exceptions by enabling the peripheral(s):
#include <xc.h>#include <sys/attribs.h>
void__ISR_AT_VECTOR (_TIMER_2_VECTOR, IPL4SRS) T2Interrupt(void){// Toggle LED LD1LATGINV = _LATG_LATG6_MASK;
// Reset interrupt flagIFS0bits.T2IF = 0;}
intmain(void){// InitializationT2CONbits.TON = 0;/* turn off Timer 2 */T2CONbits.TCKPS = 7;/* pre-scale = 1:256 (T2CLKIN = 31250 Hz) */PR2 = 3125;/* T2 period = 100mS */TMR2 = 0;/* clear Timer 2 counter */
IPC2bits.T2IP = 4;/* Set Timer 2 interrupt priority to 4 */IFS0bits.T2IF = 0;/* Reset the Timer 2 interrupt flag */IEC0bits.T2IE = 1;/* Enable interrupts from Timer 2 */
PRISS = 0x76543210;/* assign shadow set #7-#1 to priority level #7-#1 ISRs */
INTCONSET = _INTCON_MVEC_MASK;/* Configure Interrupt Controller for multi-vector mode */
__builtin_enable_interrupts();/* Set the CP0 Status register IE bit high to globally enable interrupts */
T2CONbits.TON = 1;/* Enable Timer 2 peripheral */
while(1);/* main application loop */
}
Code Example - Interrupt Usage
All preceding steps for interrupt exception usage are combined in a complete working MPLAB X IDE project:
General Exception Usage
PIC32 devices also have exception vectors for non-interrupt exceptions. These exceptions are grouped into bootstrap exceptions and general exceptions.
Bootstrap (or "Reset") Exception
A Reset exception is an exception which occurs while bootstrap code is running (StatusBEV=1).
All Reset exceptions are vectored to 0xBFC00380.
At this location, the 32-bit toolchain places a branch instruction targeting a function named _bootstrap_exception_handler(). In the standard library, a default weak version of this function is provided, which merely causes a software Reset.
If the user application provides an implementation of _bootstrap_exception_handler(), that implementation will be used instead.
The handler must be attributed with the "nomips16" attribute [e.g., _attribute_((nomips16))] since the start-up code jumps to this function.
void__attribute__((nomips16)) _bootstrap_exception_handler(void){/* Mask off ExcCode field from the Cause Register *//* Disable interrupts *//* Examine EPC and ExcCode *//* Provide a useful indication of the Exception as well as a recovery mechanism */}
General Exception
A general exception is any non-interrupt exception which occurs during program execution outside of bootstrap code (StatusBEV=0).
General exceptions are vectored to Ebase + 0x180.
At this location, the 32-bit toolchain places a branch instruction targeting a function named _general_exception_context(). The provided implementation of this function saves context, calls an application handler function (_general_exception_handler()), restores context and performs a return from the exception instruction.
A weak default implementation of _general_exception_handler() is provided in the standard library which merely causes a software Reset.
If the user application provides an implementation of _general_exception_handler(), that implementation will be used instead.
The handler must be attributed with the "nomips16" attribute [e.g., _attribute_((nomips16))] since the start-up code jumps to this function.
void__attribute__((nomips16))_general_exception_handler(void){/* Mask off ExcCode field from the Cause Register *//* Disable interrupts *//* Examine EPC and ExcCode *//* Provide a useful indication of the Exception as well as a recovery mechanism */}
Code Example - General Exception Usage
The following MPLAB X IDE project provides a simple example of general exception setup and usage :