PIC32MZ Exception Entry Points
The Reset, Soft Reset, and NMI exceptions are always vectored to location 0xBFC00000 (uncached, start-up safe KSEG1 region).
Addresses for all other exceptions are a combination of a vector base address and a vector offset.
Exception Vector Base Addresses
In MIPS32 Release 2 and higher architectures, software is allowed to specify the vector base address via the CP0 Ebase register for exceptions that occur when CP0 StatusBEV equals 0.
StatusBEV:
MIPS32 architectures provide a "bootstrap" mode (referred to as Boot-Exception Vector (BEV) mode) whereby exception entry points are reallocated into the uncached, start-up-safe KSEG1 region.
Bootstrap mode is controlled by the CP0 Status register flag StatusBEV.
- StatusBEV = 1: Exceptions vector to an uncached entry point in KSEG1: 0xBFC00xxx
- StatusBEV = 0: Exceptions vector to cached entry points in KSEG0: defined by CP0 Ebase register, plus some offset
Note: StatusBEV = 1 at reset.
The following table gives the vector base address as a function of the exception and whether the BEV bit is set in the Status register:
MPLAB XC32 start-up code initializes Ebase to the value defined by the symbol _ebase_address in the PIC32MZ device linker script (for PIC32MZ2048EFG100, _ebase_address = 0x9D000000)
Note: If Ebase is to be changed, it must be done with StatusBEV = 1 (i.e. at system boot). The operation of the CPU is UNDEFINED if Ebase is written when StatusBEV = 0.
Vector "Offsets"
Next, we have fixed vector offsets which are added to the above exception base addresses as a function of the exception:
CauseIV:
Setting the CP0 CauseIV bit to 1 causes Interrupt exceptions to use a dedicated exception vector offset (0x200), rather than having to use the general exception vector offset (0x180).
MPLAB XC32 start-up code initializes CauseIV to 1.
Final Entry Point Addresses
As seen in the above table, PIC32MZ Interrupt exception vector addresses have an additional variable offset component which is added to Ebase to form the final entry point:
Variable Offset = OFFx register value (initialized by the C-Run-time startup for each defined ISR, starting at 0x200)
We can now list the complete vector addresses for the most common exceptions (not incl. EJTAG or TLB exceptions):
Ebase:
MPLAB® XC32 start-up code initializes Ebase to the value defined by the symbol _ebase_address in the PIC32MZ device linker script (for PIC32MZ2048EFG100, _ebase_address = 0x9D000000)
Therefore, for normal interrupt operations on PIC32MZ,
- The Interrupt Exception Vector Base Address = 0x9D000000
- The Interrupt Exception Vector Final Address = 0x9D000000 + <OFFx> register value
Where,
- The first ISR's <OFFx> value is set to 0x200, and
- Subsequent ISR vector offsets (<OFFx> value) are set according to the size of the handler function(s).
For an illustration, see the multi-vector example below.
StatusEXL:
Exception Level: Set by the processor when any exception other than Reset, Soft Reset, NMI or Cache Error exception is taken
- StatusEXL = 0: Normal level
- StatusEXL = 1: Exception level; when EXL is set
- The processor is running in Kernel Mode
- Hardware and Software Interrupts are disabled
- EPC, BD, and SRSCtl will not be updated if another exception is taken
Note: StatusEXL must be cleared by the exception handler in order to re-enable interrupts. MIPS® CPUs have an instruction, eret, that both clears StatusEXL and returns control to the address stored in EPC.
Interrupt Exception Vectors
As discussed above, PIC32MZ interrupt controllers operating in Multi-Vector Mode implement a variable offset mode for calculating the final interrupt vector address:
Interrupt Exception Vector Final Address = Ebase + OFFx
MPLAB XC32 Compiler calculates & initializes the values of OFFx for each defined application interrupt service routine (see table 7.2 in the PIC32MZ data sheet for a listing of OFFx registers for each interrupt source).
The first handler is assigned 0x200 for it's OFFx register. Subsequent handler OFFx registers are initialized based upon the size of the handler functions.
Handler functions linked directly to the vector will be executed faster than those linked as the target of a dispatch function (as done on PIC32MX).
Multi-Vector Example Using Timer 2 & Timer 4 Interrupts
A small project using Timer 2 and Timer 4 to blink 2 different LEDs at different rates produced the following results for the final exception vector addresses:
Ebase:
- 0x9D000000 (initialized by the C-Run-time startup)
Timer 2 Vector Offset Register (OFF009):
- 0x200 (initialized by the C-Run-time startup)
Timer 2 Interrupt Exception Vector Final Address:
- 0x9D000000 + 0x200 = 0x9D000200
Timer 4 Vector Offset Register (OFF019):
- 0x274 (initialized by the C-Run-time startup)
Timer 4 Interrupt Exception Vector Final Address:
- 0x9D000000 + 0x274 = 0x9D000274
Here is the project for reference: interrupt-usage-multi-ef.zip