Academic Program

Alignment

Alignment

Since the PIC32MX memory system is 32-bits wide, a data access that is 32-bit (4-bytes, or  a WORD), or 16-bit (2-bytes, or a HALF-WORD) in size can either be aligned or unaligned:

  • (Naturally) Aligned Transfer: means that the data's address value is a multiple of the data's type-size (in bytes)
    • WORD size transfers are carried out to addresses that are a multiple of 4: 0x00000000, 0x00000004, 0x00000008, …
    • HALF WORD size transfers are carried out to addresses that are a multiple of 2: 0x00000000, 0x00000002, 0x00000004, …

 

  • Unaligned Transfer: means that the data's address does not follow the rules above.

 

NOTE: MIPS Release 2 requires "naturally" aligned transfers for normal load/store operations. Unaligned accesses using normal load/store operations will produce exceptions.

 

In most cases, C-compilers do not generate unaligned data accesses. It can only happen in the following cases:
 

  • Direct manipulation of pointers
  • Accessing data structures with "__packed" attributes that contain unaligned data
  • Inline/Embedded Assembly code

 

Several examples of "naturally" aligned and unaligned data transfers are shown below for a MIPS32 Little-Endian memory system:

memory-alignment.png