Virtual Address Space
The MIPS32 4 GB virtual address space is partitioned into five fixed-size segments with traditional names; different things happen according to the virtual memory area an address lies in, as follows:
KUSEG: 0x00000000-0x7FFFFFFF (low 2 GB) :
These are the addresses permitted in User mode (see Privilege Levels). In machines with a Memory Management Unit (MMU), they will always be mapped. You should not attempt to use these addresses unless the MMU is set up. On PIC32MX, this region is also cacheable.
KSEG0: 0x80000000-0x9FFFFFFF (512 MB) :
These addresses are translated directly into physical addresses by stripping off the MSB and mapping them contiguously into the low 512 MB of physical memory (0x00000000 - 0x1FFFFFFF). Since this is a "trivial" translation, these addresses are often called "unmapped". On PIC32MX, this region is also cacheable and is the default space for application code.
KSEG1: 0xA0000000-0xBFFFFFFF (512 MB):
These addresses are mapped into physical addresses by stripping off the leading 3-bits, giving a duplicate mapping into the low 512 MB of physical memory (0x00000000 - 0x1FFFFFFF). But this time, access will not use the cache.
Note that KSEG1 is the only memory region that can be used at reset because the prefetch cache must be configured by the boot code before it can be used. Therefore, your boot code must be placed in KSEG1.
KSEG2: 0xC0000000-0xDFFFFFFF (512 MB) & KSEG3: 0xE0000000-0xFFFFFFFF (512 MB) :
These areas are only accessible in Kernel mode. On PIC32MX devices, these regions are not translated to any physical memory resources. Segment KSEG3 contains the debug segment (DSEG), which is available to the EJTAG probe debugger or monitor.