Decibels (dB)
The decibel (dB) is a measure of the ratio between two quantities and is used in a wide variety of measurements in acoustics, physics, and electronics. While originally only used for power and intensity ratios, it has come to be used more generally in engineering. For instance, in electronics, we can use dB to describe the gain of an op-amp.
The use of decibels has a number of merits:
It is more convenient to add the decibel values of two consecutive amplifiers rather than to multiply their amplification factors.
Decibels are useful because they allow even very large or small ratios to be represented with a conveniently small number (similar to scientific notation). This is achieved by using a logarithm, allowing one to clearly visualize huge changes of some quantity. The formula below shows that dB can be used to describe the op-amp gain (A).
A(dB) = 20 log (Vout/Vin)
For example, if the open-loop gain of an op-amp is 100 dB, we have 100 dB = 20 log (Vout/Vin)
100 / 20 = log (Vout/Vin)
5 = log (Vout/Vin)
(Vout/Vin) = 100 000
If the input changes by 1 V, the output changes by 100 000 V. This demonstrates the high open-loop gain of an op-amp. Realistically, the op-amp output goes to the rail if the inputs change by 1V. Assuming the rail is 5 V, it only takes the input voltage change by 5 / 100 000 = 50 uV for the op-amp to go to the 5 V rail.