Academic Program

Programming a Development Board

Programming a Development Board

In order to apply the concepts you've just learned, watch the following video to see how to open an existing sample project, build the project, and program the application firmware into a PIC18F47Q10 microcontroller running on a Curiosity HPC Development Board

The project will demonstrate how the MCU can toggle the D2 LED on the Curiosity HPC Development board On/Off every 250 milliseconds.

Hardware Tools


Curiosity HPC Development Board

About Buy

Project Download


Download the example project. Download