Academic Program

Macros

Macros

Macros are text replacements created with #define that insert code into your program. Macros may take parameters like a function but the macro code and parameters are always inserted into code by text substitution.

Macros:

  • Are evaluated by the preprocessor
  • Are not executable code themselves
  • Can control the generation of code before the compilation process
  • Provide shortcuts

Simple Macros

Syntax

​

#define label text

  • Every instance of label in the current file will be replaced by text
  • text can be anything you can type into your editor
  • Arithmetic expressions evaluated at compile time

Example

1
2
3
#define Fosc 4000000
#define Tcy (4 * (1/Fosc))
#define Setup InitSystem(Fosc, 250, 0x5A)

Argument Macros

Syntax

​

#define label(arg1,…, argn) code

  • The code must fit on a single line or use "\" to split lines
  • Text substitution used to insert arguments into code
  • Each instance of the label() will be expanded into code
  • This is not the same as a C function

Example

1
2
3
#define min(x, y) ((x)<(y)?(x):(y))
#define square(x) ((x)*(x))
#define swap(x, y) { x ^= y; y ^= x; x ^= y; }

Extreme care must be exercised when using macros. Consider the following use of the below macro:

1
#define square(a) ((a)*(a))
1
2
i = 5;
x = square(i++);

The result will be the following:

​

x = 30
i = 7

​

Wrong Answers!
x = square(i++);
expands to:
x = ((i++)*(i++));
So i gets incremented twice, not once at the end as expected.