Academic Program

Lab Exercise 18: Enumerations

Objective

This demo illustrates the use enumerations to create a list of constant labels that may be used in conjunction with variables declared with the enum’s type. The primary purpose of enumerations is to make your code more readable and easier to maintain.

Software Tools

Tool ‍ About Installers
‍
Installation
Instructions
‍ Windows ‍ Linux ‍ Mac OSX
‍
MPLAB® X
Integrated Development Environment
‍ ‍ ‍ ‍ ‍
‍
MPLAB® XC16
C Compiler
‍ ‍ ‍ ‍ ‍

Exercise Files

File Download
‍
Installation
Instructions
‍ Windows ‍ Linux ‍ Mac OSX
‍
Project and Source Files
‍ ‍ ‍ ‍

 

Procedure

Open the Project

Start MPLAB® X IDE, then click on the Open Project Main_Open_Project.png icon on the main toolbar

Navigate to the folder where you saved the exercise files for this class.

Click on the Lab18.X folder.

Select Open Project .
 

Debug Project

Click on the Debug Project Main_Debug_Project.png button. This will build and send the program to the simulator.
Click on the Continue Debug_Continue.png button. This begins the simulation.Wait for the UART 1 Output window to finish printing.
Click on the Halt Debug_Pause.png button.

Results

Lab18Results.png

 

After running the program, the UART1 Output window should display the text: “Bandpass filter selected.”

 

Code Analysis

Line 13
An enumeration data type called filterTypes is defined. This line essentially defines the following constants:
BANDSTOP = 0
LOWPASS = 1
HIGHPASS = 2
BANDPASS = 3
declared to be of type filterTypes.

Line 18
This line declares a variable called filter of type filterTypes. Some compilers will restrict this variable to holding just the values defined by the enumeration, though it isn’t always the case. At the very least, it will make your code easier to read and maintain by associating a group of constants with a particular variable.

Line 34
Here, we initialized the variable filter to BANDPASS. This effectively assigns a value of 3 to the variable, which may be used as any ordinary integer type variable.

Line 36-42
These lines simply call a particular function depending on the value of the variable filter. Notice that in every place that a constant would be used, we have used on of the labels defined in the enumeration type declaration.
The functions themselves are defined in the file Utilities.c, and all they do is print out which filter was selected to the SIM UART 1 window.

End Debug Session

End the Simulation Session by clicking the Finish Debugger Session Debug_Finish_Debugger_Session.png button.

Clear out the UART 1 Output window (Ctrl + L)

Close the Project.

Conclusions

Enumerations provide a means to associate a list of constants with one or more variables. Theoretically, these constants represent the entire range of valid values for the variable. Some compilers will enforce this range (compile time only - runtime checking is up to you). However, even if the compiler doesn’t do any checking, by sticking to the list of valid constants it becomes more difficult to accidentally assign an invalid value.

Perhaps the greatest benefit of using enumerations is that they make your code more readable by replacing “magic numbers” and that it becomes much easier to maintain. If you need to add additional valid values, you need only add them to the enum list. If the values of some of the labels change, you may not have to change the rest of your code to reflect the changes (depending on how you have written your code).