Overflow and Saturation
The dsPIC supports two optional saturation modes that affect the output of the 40-bit adder: 32-bit Saturation (referred to as Normal Saturation) and 40-bit Saturation (referred to as Super Saturation). Selecting the saturation mode is controlled by several bits in the CORCON register. The SATA bit enables or disables saturation for Accumulator A, and the SATB bit enables or disables saturation for Accumulator B. When saturation is enabled, the ACCSAT bit is then used to select the type of saturation - either Normal Saturation or Super Saturation. The same saturation mode will apply to both accumulators if both SATA and SATB are 1. Lastly, there is a SATDW bit in the CORCON that enables Data Write Saturation. This feature allows for the “best possible” 16-bit value to be stored from the accumulator when the SAC instruction is used.
- Overflow
- Passively sets a corresponding status bit indicating that overflow has occurred
- Saturation
- Actively limits the maximum size of data and preserves sign bit
- Saturation modes
- Selected by CORCON
- None (Default):
- Calculation results will be allowed to destroy sign bit (bit 39), no trap set
- Catastrophic:
- Arithmetic trap when sign bit (bit 39) destroyed
- Normal Saturation:
- Bit 31 Overflow and Saturation
- Super Saturation:
- Bit 39 Overflow and Saturation
Saturation Control
CORCON: Core Control Register
| U-0 | U-0 | U-0 | R/W-0 | R/W-0 | R-0 | R-0 | R-0 |
| — | — | — | US | EDT | DL2 | DL1 | DL0 |
| bit 15 | bit 8 |
| R/W-0 | R/W-0 | R/W-1 | R/W-0 | R/C-0 | R/W-0 | R/W-0 | R/W-0 |
| SATA | SATB | SATDW | ACCSAT | IPL3 | PSV | RND | IF |
| bit 7 | bit 0 |
| Legend | ||
| R = Readable Bit | W = Writable Bit | U = Unimplemented bit, read as '0' |
| u = Bit is unchanged | x = bit is unknown | -n/n = Value at POR and BOR/Value at all other resets |
| '1' = bit is set | '0' = bit is cleared | -n = Value at POR reset |
bit 15-13 Unimplemented: Read as '0
bit 12 US: DSP Multiply Unsigned/Signed Control bit
bit 11 EDT: Early DO Loop Termination Control bit
bit 10-8 DL<2:0>: DO Loop Nesting Level Status bits
bit 7 SATA: AccA Saturation Enable bit
1 = Accumulator A saturation enabled
0 = Accumulator A saturation disabled
bit 6 SATB: AccB Saturation Enable bit
1 = Accumulator B saturation enabled
0 = Accumulator B saturation disabled
bit 5 SATDW: Data Space Write from DSP Engine Saturation Enable bit
1 = Data space write saturation enabled
0 = Data space write saturation disabled
bit 4 ACCSAT: Accumulator Saturation Mode Select bit
1 = 9.31 saturation (super saturation)
0 = 1.31 saturation (normal saturation)
bit 3 IPL3: CPU Interrupt Priority Level Status bit 3
bit 2 PSV: Program Space Visibility in Data Space Enable bit
bit 1 RND: Rounding Mode Select bit
bit 0 IF: Integer or Fractional Multiplier Mode Select bit
Saturation Disabled
When saturation is disabled, the output of the adder is never modified. In this mode, the adder provides the same dynamic range as with Super Saturation mode, namely -256.0 to approximately +256.0, but no clipping will occur when this range is exceeded. When an operation exceeds the allowed range, the lower 40 bits of the result will remain unchanged, even though they would be incorrect. This condition is called a “Catastrophic Overflow”, and the user has the option of having this generate a Math Error Trap. This selection is controlled by the Catastrophic Overflow Trap Enable bit, which resides in the INTCON1 register.
- ACCxU contains magnitude data
- Fixed-point range of (-256.0 - ~+255.0)
- Results are never modified
- If sign-bit (bit 39) is destroyed
- Overflow bit for Corresponding accumulator is set
- Trap will be generated if trap is enabled
- Default
Saturation Trap Control
INTCON1: Interrupt Control Register 1
| R/W-0 | U-0 | U-0 | U-0 | U-0 | R/W-0 | R/W-0 | R/W-0 |
| NSTDIS | — | — | — | — | OVATE | OVBTE | COVTE |
| bit 15 | bit 8 |
| U-0 | U-0 | U-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 | U-0 |
| — | — | — | MATHERR | ADDRERR | STKERR | OSCFAIL | — |
| bit 7 | bit 0 |
| Legend | ||
| R = Readable Bit | W = Writable Bit | U = Unimplemented bit, read as '0' |
| u = Bit is unchanged | x = bit is unknown | -n/n = Value at POR and BOR/Value at all other resets |
| '1' = bit is set | '0' = bit is cleared | -n = Value at POR reset |
bit 15 NSTDIS: Interrupt Nesting Disable bit
bit 14:11 Unused: Read as '0
bit 10 OVATE: Accumulator A Overflow Trap Enable bit
1 = Trap overflow of Accumulator A
0 = Trap disabled
bit 9 OVBTE: Accumulator B Overflow Trap Enable bit
1 = Trap overflow of Accumulator B
0 = Trap disabled
bit 8 COVTE: Catastrophic Overflow Trap Enable bit
1 = Trap on catastrophic overflow of Accumulator A or B enabled
0 = Trap disabled
bit 7:5 Unused: Read as '0
bit 4 MATHERR: Arithmetic Error Status bit
bit 3 ADDRERR: Address Error Trap Status bit
bit 2 STKERR: Stack Error Trap Status bit
bit 1 OSCFAIL: Oscillator Failure Trap Status bit
bit 0 Unimplemented: Read as '0
Normal Saturation (31-bit)
The Normal Saturation mode supports a 1.31 data format. The 1.31 data format uses just one magnitude bit (which is a sign bit) and 31 fractional bits to represent a value. When Normal Saturation is enabled, the output of the adder is limited to a range of 32 bits, and Accumulator Upper contains the sign-extension of the 32-bit value stored in Accumulator High and Accumulator Low. The sign of the 32-bit value, stored in Accumulator High bit 15, is extended to all bits in Accumulator Upper. This means that if an operation destroys the sign-bit stored in Accumulator bit 31, the Adder will saturate the result to either the largest 32-bit negative number or the largest 32-bit positive number.
- Output of adder uses 32 bits only
- Sign bit (ACCx<31>)extended into ACCxU
- Resultant sign bit is preserved during subsequent operations
- Overflow will never occur
- Accumulator will saturate instead of overflow
- Fractional mode result is sign extended 1.31
Largest positive value is 0x00 7FFF FFFF (0.999969482422)
Largest negative value is 0xFF 8000 0000 (-1.000000000000)
Super Saturation (39-bit)
When Super Saturation is enabled, the output of the Adder is limited to a range of 40 bits, and the Accumulator Upper register contains the upper 8-bits of magnitude information. This data format is referred to as 9.31, because it has 9 magnitude bits, which includes one sign bit, and 31 fractional bits. In Super Saturation mode, when an add operation destroys the sign-bit stored at Accumulator bit 39, the Adder will saturate the result to either the largest 40-bit negative number or the largest 40-bit positive number. The maximum negative Accumulator value is 0x8000000000 or -256.0 as a fixed-point value. The largest positive Accumulator value is 0x7FFFFFFFFF or approximately +256.0. The Super Saturation mode provides computational head room which may be very useful in algorithms, while simultaneously providing system protection from runaway calculations. The accumulator value can increase and decrease as long as the value is within the range of -256 and +256.
- Largest positive value is 0x7F FFFF FFFF (+255. 999969482422)
- Output of adder uses 40 bits
- Overflow in this mode is detected by STATUS bits
- Integer mode magnitude grows into ACCxU
- Fractional mode magnitude grows but:
- Implied radix point remains between bits ACCxH<31> and ACCxH<30>
- 1.31 format is magnitude extended to 9.31
- When sign bit 39 clobbered, saturation logic
- Retains sign bit in bit 39
- Fills all other bits in accumulator with maximum positive or negative value
Saturation Detection
SR: CPU STATUS Register
| R-0 | R-0 | R/C-0 | R/C-0 | R-0 | R/C-0 | R-0 | R/W-0 |
| OA | OB | SA | SB | OAB | SAB | DA | DC |
| bit 15 | bit 8 |
| R/W-0 | R/W-0 | R/W-0 | R-0 | R/W-0 | R/W-0 | R/W-0 | R/W-0 |
| IPL2 | IPL1 | IPL0 | RA | N | OV | Z | C |
| bit 7 | bit 0 |
bit 15 OA: Accumulator A Overflow Status bit
1 = Accumulator A overflowed
0 = Accumulator A has not overflowed
bit 14 OB: Accumulator B Overflow Status bit
1 = Accumulator B overflowed
0 = Accumulator B has not overflowed
bit 13 SA: Accumulator A Saturation ‘Sticky’ Status bit
1 = Accumulator A is saturated or has been saturated at some time
0 = Accumulator A is not saturated
bit 12 SB: Accumulator B Saturation ‘Sticky’ Status bit
1 = Accumulator B is saturated or has been saturated at some time
0 = Accumulator A is not saturated
bit 11 OAB: OA or OB Combined Accumulator Overflow Status bit
1 = Accumulators A or B have overflowed
0 = Neither Accumulators A or B have overflowed
bit 10 SAB: SA or SB Combined Accumulator ‘Sticky’ Status bit
1 = Accumulators A or B are saturated or have been saturated at some time in the past
0 = Neither Accumulator A or B are saturated
bit 9 DA: DO Loop Active bit
bit 8 DC: MCU ALU Half Carry/Borrow bit
bit 7-5 IPL<2:0>: CPU Interrupt Priority Level Status bits
bit 4 RA: REPEAT Loop Active bit
bit 3 N: MCU ALU Negative bit
bit 2 OV: MCU ALU Overflow bit
bit 1 Z: MCU ALU Zero bit
bit 0 C: MCU ALU Carry/Borrow bit