Modify main.c
Double click on the main.c file. It opens in the editor window.
We need to add the following code to the main.c file.
void main(void)
{ // initialize the device SYSTEM_Initialize();
while (1)
{
// Add your application code
if (switch_GetValue() == 0)
{
led_SetHigh();
}
else
{
led_SetLow();
}
}
}
MCC automatically generates switch_GetValue(), led_SetHigh() and, led_SetLow(). You can find them in the pin_manager header file.
Next, click on the Build Main Project icon to compile the code. You will see a BUILD SUCCESSFUL message in the output window.