Academic Program

PID Basics: dsPIC® DSC Implementation Part 3

PID Basics: dsPIC® DSC Implementation Part 3

PID Term Computation Continued

7) Moves the content of the RAM location pointed to by W8 into register W4.

8) Moves the content of the RAM location pointed to by W10 into register W5.

PID-operation-11-new.png

9) Updates the W10 register, so that it is now pointing to the previous RAM location.

PID-operation-12-new.png

Store Accumulator Instruction

The diagram below shows the operation of the store accumulator instruction, sac.r.

PID-operation-13.png

1) We store the high part (from 16th to 31st bit) of the accumulator into the W0 register. Before saving it, the value is shifted 8-bit positions to the left and the resultant value is rounded. See diagram below.

PID-operation-14.png

2) Copy the content of register W5 [that is e(n-1)] into the last location of the error buffer.

PID-operation-15.png

3) The content of RAM location pointed to by [W10 -4] is then copied into the W5 register.

PID-operation-16.png

4) The pointer W10 is decremented, to point to the previous location of the error buffer.

PID-operation-17-new.png

5) The content of register W5 (that is the current error e(n)) is stored into the RAM location pointed to by W10. The purpose of the operations performed in the last few diagrams is to make room for the next value of the error that will arrive in the next sampling period.

PID-operation-18-new.png

 

Example

The number of cycles required to perform the PID operations as indicated in the previous diagrams can be explained using the following example:

If the dsPIC® DSC is running at 40 MIPS, each machine cycle equals: 1/40 MHz = 25 ns. As a consequence, the total time required to perform the described task is 13 x 25 ns = 325 ns.