Academic Program

CWG Example Operation

CWG Example Operation

The CWG example is running and the screen capture below shows the results.
The NCO signal can be seen at the top of the screen capture along with the CWGA and CWGB signals. You can also see the dead-band delays that are triggered by the edges of the NCO input signal.

exp10.png

The CWG is forced into Shutdown mode.
When the momentary switch is pressed, the CWG outputs are driven to their inactive state showing the shutdown has occurred.

exp11.png