Complementary Waveform Generator Example
This page is a step by step example that uses the Complementary Waveform Generator (CWG).
This example uses the Numerically Controlled Oscillator (NCO) output signal (running at 50% duty cycle) as the input and the High-Frequency Internal Oscillator (HFINTOSC) as a clock.
This example also produces two complementary outputs and uses an external switch as the shutdown control, as shown in the block diagram below.