Academic Program

Introduction to the 8-bit PIC MCU Timer0

About this course

This training will introduce you to the Timer0 peripheral that is available on all Microchip 8-bit PIC® MCU devices. Three chapters are included:

  • Introduction
  • Timer0 Operation
  • Project Example

The Introduction chapter (that you are in now) will introduce the Timer0 structure.

The Timer0 Operation chapter will explain the different operational features of Timer0.

The Project Example chapter will show a simple example of using Timer0.

At the end of this training, you will have a basic understanding of the Timer0 peripheral and how it can possibly work in your application.

After you have read through a lesson within a chapter, press the Next button to advance to the next lesson. 

At the end of each chapter, you will be shown the status of your progress and take a brief knowledge check before moving on to the next section.