Academic Program

Decision Statements

Following is the general form of a typical decision-making structure found in most of the programming languages:

ifStatement.png

 

C programming language assumes any non-zero and non-null values as True, and if it is either zero or null, then it is assumed as a False value.

C programming language provides the following types of decision-making statements:

Statement Description
if statement An if statement consists of a Boolean expression followed by
one or more statements.
if … else statement An if statement can be followed by an optional else statement,
which executes when the Boolean expression is False.
nested if statements You can use one if or else if statement inside another if or else
if
 statement(s).
switch statement switch statement allows a variable to be tested for equality
against a list of values.
nested switch statements You can use one switch statement inside another switch
statement(s).